|
|
|
Kaydon
Bearings, the world's leading
manufacturer of thin section bearings, sets the industry
standard. RealiSlim bearings are ideal for applications in
aviation, aerospace, robotics, machine tools, semiconductor
manufacturing, or medical equipment, or anywhere a lighter,
thinner bearing is required. |
|
Industrial
Tectonics Inc. manufactures specialty high-
precision balls
from .005" to 10" diameter,
which are ideal
for applications ranging from petrochemical to
the nuclear
industry.
ITI maintains
the world's largest selection of
stock
specialty balls
and can also custom manufacture from
hundreds of materials to
a customer's specifications.
|
| |
|
|
|
|
|
| Kaydon
Filtration Group designs and builds industrial oil
filtration equipment and fuel filtration equipment for markets
such as
power generation, Military Fuel Handling, Pulp & Paper,
Steel, Marine, Mining, Cryogenic, Fluid Power and Machine Tool. |
|
Kaydon
Rings and Seals is the full line supplier for your
turbomachinery shaft seal requirements and the premier
designer
and manufacturer of piston rings. From labyrinth
to oil seals
to dry gas seals, Kaydon does it all. Extensive
testing
has verified the designs and field experience has
solidified
Kaydon's
position as
the piston ring manufacturer
of choice.
|
|
|
|
| Spirolox More
design engineers are specifying Spirolox compression wave springs
and Spirolox retaining rings for thousands of applications. spirolox
offers standard spiral-wound retaining rings made from carbon and
stainless steel in diameters from 7/16" to 15" for light,
medium, and heavy-duty applications, internal or external. Need
engineering assistance, or want to order? Get your FREE Custom
Quote today |
|
Cooper is
the world's number one Split Bearing Company.
Cooper customers
around the world are delighted with the
optimum performance the
Cooper bearing provides. Able to
operate in hostile and difficult
operating conditions proves no
obstacle for the proven Cooper product
operating in various
industries around the world. |
| |
|
|
|
|
|
| Canfield
Technologies, manufactures a complete line of tin/lead
alloys for many applications. They are capable of making all
of the industrial solder alloys available and can custom make
an alloy for your specific needs. They furnish these products
in cast bar of various weights and sizes. Extruded bar is also
available, but the sizes available are dependent on the ability
and die design. |
|
Indiana
Precision, Inc. exists to provide quality, ultra-
precision
tooling, fixtures, gauges and components to its
customers,
along with a prototyping and problem solving
mindset that says... "Yes!
It can be done! |
| |
|
|
|
|
|
| Purafil For
- over 30 years, Purafil has been the world leader in the engineering
and manufacture of gas-phase air filtration media, systems, and
air quality monitors. Purafil revolutionized the gas-phase air
filtration industry with the development of the world's first potassium
permanganate, air-cleaning media. Today Purafil is providing innovative,
clean air solutions to customers in every geography and market.
Purafil is supported by representative firms throughout the United
States and over 50 countries. |
|
Tridan
International Inc., is a world leader in the supply
of
machinery for the production of evaporators and condensers
commonly used in manufacturing air conditioning and refrigeration
systems. Since 1966, machinery designed and built by Tridan
has been supplied to more than 900 customers in over 60
countries
throughout the world. |
| |
|
|